Issue:
This article answer the question of, Can I power the ACSC1XX unit from a UPS.
Product line:
ACSC1XX.
Environment:
All Serial Numbers.
Cause:
FAQ.
Resolution:
The SC should be powered from a dedicated circuit; the unit has very high in-rush current (>55 amps) that may overload the UPS every time the compressor turns on. If you must power the SC from a UPS, then it needs to be properly sized; a dedicated UPS would be preferred. Contact your Config team rep or Systems Engineer for additional assistance.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.