Browse FAQs

Only one NetBotz appliance at a time can monitor a Pelco Camera

Published date: 21 July 2020

Issue:

When more than one NetBotz appliance monitors the same Pelco camera, Pelco camera event notifications and motion detection seem to intermittently fail.

Product Line:

NetBotz, Pelco

Environment:

NetBotz software Interfaces

Cause:

Users are allowed to discover the same Pelco camera on more than one NetBotz appliance. No warning message is displayed

Resolution:

Users should not discover the same Pelco camera on more than one NetBotz appliance. Removing from both NetBotz appliances and re-adding to the one appliance that will be used to monitor the Pelco camera may be required to regain proper motion detection notification.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.