Consulter la FAQ



Where are your NetworkAIR ACFM manuals?
NetworkAIR FM DX, Precision , CRAC, Perimeter, CRAH ... , acfm400, Air-cooled, Water -cooled, Glycol-cooled
Uniflair Humidifier Water Quality
When the current falls below the value required ... result of the fall in the water level, the feed water solenoid valve is opened.
What does water collection pan full mean and how do I fix it?
... tube should face downward as the water exiting the condensate tube should be able to fall freely (the ... be submerged in water ).
NetworkAIR FM Secondary Compressor Lock Out
NetworkAIR FM Secondary Compressor will not Turn On : Under low return air temperature conditions, low evaporator load results in a new lower system balance temperature for the evaporator coil. • Evaporator dirty
How to navigate through an Network Air FM unit display
System Configuration The System configuration options are ... Modules in the System ... ... damage to your System . Some System configuration settings may ... NetworkAIR FM DX Precision Air Conditioner. System options ... > Setup > System # > System Config > System Options The System Options ... installed in this System and the methods ... ... required for this System . ... components in the System .and is ... ... Modules of this System . ... ® (chilled water ) and DX ... The System can control the ... ... ): The System activates humidification modes ... – The System activates humidification based ...
What are the operational conditions for an InRoom (Stulz) Unit
The InRoom precision air conditioning units operate within the following ranges: ... Chilled water -/cooling water pipes: Maximum water head pressure: 10 bar (145 psi) ... Entering water temperature (EWT) for CW coil: 7°C (44.6°F) Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Chilled water medium (CW): 0% Glycol
What is Modbus and How does it work?
32-bit double precision IEEE floating point number ... Therefore, some manufacturers implemented modbus in their equipment to store and transmit the higher byte first followed by the lower byte. ... Alternatively, others store and transmit the lower byte first ( ... The limit defined in the modbus specification is even lower at 247.
Refrigerant charging table for a Uniflair Unit
• All refrigerant lines/chilled water piping are free from debris. ... premature joint failures due to system vibrations. ... Refrigerant velocity must be high enough to keep oil entrained in the flow to ensure the proper flow of oil throughout the system , in particular when operating at partial load. ... If the refrigerant velocity is too high, both the noise level and pressure drop will increase. ... Liquid lines must be sized to ensure sufficient refrigerant flow to the expansion device and to minimize pressure drop .
EcoBreeze Variable Speed Drive Technical Spec’s
Asynchronous motor control Factory set : constant torque Sensorless flux vector control with PWM type motor control signal ... Relative humidity 5...95 % without condensation conforming to IEC 60068-2-3 5...95 % without dripping water conforming to IEC 60068-2-3
Network Air FM unit spare parts list
25 Pin Cable Lower (Downflow) ... 25 Pin Cable Lower (Upflow) ... 875-4183 Glycol/ Water LL ... 875-4182 Glycol/ Water & Air LL ... HEAT EXCHANGER - FM NAM 35KW WATER , R22 ... HEAT EXCHANGER - FM NAM 40kw WATER , R22 ... HEAT EXCHANGER - FM NAM 50kw WATER , R22 ... Rope Water Detector Assembly (0w1586 cable only) ... Spot Water Detector (Assy. ... Water Flow Switch Assy


Résultats 1 - 10 de 69

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.