Consulter la FAQ

Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL

Date de publication : 11 September 2020

Issue:
Where to find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL
 

Product line:
SYBTU1-PLP / SYBTU2-PLP, GVSBTU/GVSBTHU/GVSBTHULL
 

Environment:
PX1,2, 250-500, SUVT, Galaxy 3500, Galaxy VS
 
 
Information:
See application note 143 for specific values of contained electrolyte in both the SYBTU1-PLP (used in PX1 20,40, 48, 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and the SYBTU2-PLP (used in the PX2 100KVA and the PX 250/500KVA UPS units) batteries.

Application Note 143:
https://www.apc.com/salestools/SMCR-6NXGXU/SMCR-6NXGXU_R2_EN.pdf
 
 
Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. For further information on MSDS by the specific vendors please refer to FA157067
 
 Also see FA157067

Galaxy VS Modular Batteries:
 
Battery Type Electrolyte Weight Electrolyte Volume
(kg) (lbs) (ml) (gal)
GP1272F2FR 0.5 1.11 378 0.1
HR1234WF2FR 0.44 0.98 333 0.09
UP-PW1245P1 0.4794 1.057 378 0.0998
         
Battery Type Electrolyte Weight Electrolyte Volume
(kg) (lbs) (ml) (gal)
GVSBTU 5 11.1 3780 1
GVSBTHU 4.4 9.8 3330 0.9
GVSBTHULL 4.794 10.57 3780 0.998
         
Battery Type Electrolyte Weight Electrolyte Volume
(kg) (lbs) (ml) (gal)
GVSBT4 20 44.4 15120 4
GVSBTH4 17.6 39.2 13320 3.6
GVSBTH4LL 19.176 42.28 15120 3.992

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.