Browse FAQs



NetBotz | Hardware & Software Support Information and Limits
... Hardware Warranty & Software Support The NetBotz Rack Appliances 750 has a software /hardware support limitation of 5 years (2 years factory with 3 years of purchasable extensions ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 Software Support & Hardware Support Factory Warranty Out of Support Out of Support The NetBotz Rack Appliances 250 has a software /hardware support limitation of 5 years (2 years factory with 3 years of purchasable extensions ... Year 1 Year 2 Year 3 Year 4 Year 5 Year 6 Software Support &
Did APC purchase the AirFlow Company?
Data Center Cooling ... purchased Airflow in 2000 and formed a ... American Power Conversion Expands Availability Solutions with Acquisition of Airflow Company ... October 23, 2000 - American Power ... ... , global, one -stop shop ... ... specifically designed for applications that are sensitive ... IT and telecommunications applications . ... a variety of applications including datacenters, ... ... solutions also offer one of the smallest ... ... the fourth quarter 2000 this transaction is ... ... Airflow’s fiscal year 2000 revenue was $ ... ... and Advance Power’s operations ; the timely ... of global manufacturing capacity ; general worldwide ... ... equipment, related software , professional and ... ... West Kingston, Rhode Island, reported sales of $ 1 .337 billion for ...
APC Security Advisory - InfraStruxure Central 5.0 Java Runtime Environment
... processing of XML Data . [ 1 ] ... processing of XML data may allow unauthorized ... ... with processing XML data may allow an untrusted applet or application that is downloaded ... ... of malicious XML data ... uploading of XML data , the data must adhere to ... ... untrusted applet or application to elevate its ... ... or execute local applications that are accessible ... ... Central Client uses one font throughout all ... ... Environment Scripting Language Support . ... to scripting language support may allow an untrusted applet or application to elevate its ... ... or execute local applications that are accessible ...
APC Security Advisory - Static Factory Password Vulnerability
... or device has one of these cards ... ... manual for further information . ... to a newer application revision that has ... at the same application revision for those ... ... devices with network support are affected. ... Description AOS Rev APP Rev AOS Rev APP Rev Smart- ... ... mx28 110 Switched Rack PDU aos 116 ... ... The AOS and APP firmware revisions listed ... ... _hw02_ APP _REV. ... ... both AOS and APP revsions are available ... ... Description AOS Rev APP Rev AOS Rev APP Rev Smart- ... ... The AOS and APP firmware revisions listed ... ... or device has one of these cards ...
INFORMATION BULLETIN: Potential Issue with AP8XXX series Rack Power Distribution Units with rpdu2g v6.0.9 firmware
... , the rest of the firmware modules (AOS, rpdu2g application module) need to be loaded by one of the methods available here ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
3. Run a terminal program such as HyperTerminal ... bps, 8 data bits, no parity, 1 stop bit, and no flow ...
APC Security Advisory - Java Runtime Environment Unsigned Applet Privilege Escalation
1 . Ensure that ... ... C:\ Program Files\java Registry: data path in my ... \Parameters\ Application NOTE: ... instance number is 1 e.g ... ... C:\ Program Files (x86 ... Registry: data path in my ... \Parameters\ Application NOTE: ... instance number is 1 e.g ... 1 . Stop the ... 1 . Uninstall PowerChute ... A STAND -ALONE COPY ... MAY LACK IMPORTANT INFORMATION OR CONTAIN FACTUAL ... ... IMPLEMENTATION OF THE INFORMATION CONTAINED HEREIN HOWEVER ... AN ACTION FOR CONTRACT , STRICT LIABILITY ... ... unmodified, and include all date and version information .
Data Center Expert | How do I upgrade my software version?
Process for upgrading StruxureWare Data Center Expert. ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465) ... StruxureWare Data Center Expert (all versions) ... You must have a valid currently active software support contract to receive upgrade files. ... 1 ) Download the upgrade.zip ... Upgrades usually take an hour or less to complete, but for certain upgrades it may take significantly longer depending on the number of devices and amount of historical data .
Rack PDU 2G (AP8XXX) Network Port Sharing Information
General information regarding the Network ... Capability of AP8XXX Rack PDU models Rack Power Distribution AP8XXX Rack PDU series only ... ability to share one IP address via one network connection) General information ... to the detailed information sections below. ... up to four Rack PDUs using only one ... by connecting the Rack PDUs via the ... ports on the Rack PDU front panel ... All Rack PDUs in the ... using the same Rack PDU firmware revision ... in order to support the Network Port ... ... a number, 1 to 4, ... uniquely identify the Rack PDUs in a ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.