Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
Product Line: StruxureWare Data Center Expert (DCE)
Data Center Expert | How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
... Upon launching the StruxureWare Data Center Expert client an error ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465 ... StruxureWare Central (SWC ... StruxureWare Client (potentially ... StruxureWare may be attempting ... 1 ) Navigate to the Installation directory for StruxureWare Data Center Expert . (default directory is: C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X.X) ... -vm "C:\ Program Files (x86)\ StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe"
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... to gather specific information about the alert ... 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine
Data Center Expert | How do I upgrade my software version?
Product Line StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465)
Data Center Expert | Application Version does not update in the UI after upgrading devices to AOS 6.4.6 and newer
Product Line StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465)
Is StruxureWare DCE or NetBotz vulnerable to CVE-2017-7494 (Samba related vulnerability)?
Are StruxureWare DCE or NetBotz ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all versions) ... Experts say the vulnerability can be exploited with just one line of code and has the potential to spread quickly. Samba versions 3.5 (released March 1 , 2010) and onwards are impacted. ... StruxureWare DCE v7.X runs on Linux but does not export SMB shares, so it is not vulnerable. ... Cyber Security is an important element of Schneider Electrics' commitment to software quality.
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
1 . Open the application 2. Enter IP address or hostname within the "Host Name" field
Data Center Expert | How do I enable SSL communication between StruxureWare and multiple Netbotz devices?
StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465 ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... Struxureware Data Center Expert and Netbotz Communication ... Struxureware Data Center Expert (SWDCE) ... received from any one Netbotz device. Information retrieved from each ... may include alarm data , configuration data , or surveillance data . ... will now POST information to the SWDCE ... alarm or other data . ... will show status information on all devices ... ... you can create one discovery for the ... ... /Post Alert Data Settings.
Data Center Expert | Restoring backup to a new Virtual Machine causes system to not fully boot up.
... demo version OVA, and configure it using the hardware equivalents for the StruxureWare Data Center Expert Basic , Standard, or Enterprise server from ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.