Browse FAQs

Why is the Start and End Time in the Graph and History View under Netbotz Advanced View is limited to 8 hours?

Published date: 09 December 2019

Issue:
Start and End time for the Graph and History view is limited to 8 Hours.


Product Line:
Netbotz V3

Environment:
Netbotz 4xx, 5xx devices

Cause:
Default storage capacity for Netbotz Version 3 appliance.
 
Resolution:
Add external storage (e.g. remote network folder or USB drive).
Without any external storage added, the Netbotz appliance can only interpret sensor readings 8 hours from the time the graph and the history report is generated.
To add external storage to the Netbotz v3 appliance, you can refer to the article FA360166 for the complete instructions. Once external storage is added, earlier options for the “start time” drop-down menu will be available.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.