StruxureWare Central (SWC)
InfraStruXure Central (ISXC)
Environment:
StruxureWare Data Center Expert (All Versions)
Cause:
Issues may occur with StruxureWare Data Center Expert that require the server to be restored to defaults and a backup to be restored on it (if available). This is usually done per a request from Data Center Expert technical support.
1) Download and deploy the OVA (provided by technical support) for the same exact version of Data Center Expert that the last backup was created on. Instructions for deploying a virtual appliance can be found in knowledge base FA299551, just ensure to use the download provided from technical support. NOTE: Assign the Virtual Appliance the same MAC as the old virtual appliance. If this is not possible, let VMWare choose a MAC address and then contact technical support after completing step 2.
2) Assign the network settings on the appliance, per instructions found in knowledge base FA234266. NOTE: Keep in mind any IP Address restrictions within the network management cards SNMP settings or network firewalls that may prevent communication from working properly.
1) Contact technical support and they will provide the restore ISO for your server.
2) Create a bootable USB restore key following the instructions inside of the download provided by technical support. NOTE: If you are restoring a version prior to 7.4.X the maximum size of the USB drive is 4GB. NOTE: Ensure to use an elevated command prompt (run as Administrator) when creating the USB restore key.
3) Insert the created USB restore key into a USB port located on the back of the physical appliance.
4) Connect a keyboard and monitor to the appliance.
5) Reboot the server and select to boot from the USB Drive (select boot options when the server is starting).
6) Assign the network settings on the appliance, per instructions found in knowledge base FA234266. NOTE: Keep in mind any IP Address restrictions within the network management cards SNMP settings or network firewalls that may prevent communication from working properly.
1) Log into your DCE desktop client to the appliance.
2) Navigate to the System Menu > Server Administration Settings > Server Backup/Restore.
3) Click on Restore From Backup.
4) Select New Backup Location. NOTE: If you did not perform a reset to defaults, select Existing Backup Location and skip to step 8.
5) Select Windows Share or NFS share, click Next. Fill in the required information and click Next. NOTE: Instructions on setting up a Windows share to work with Data Center Expert can be found in knowledge base FA299440.
6) Select the backup to restore from and click Finish.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.