Browse FAQs

Files to gather when troubleshooting PowerChute Network Shutdown 3.1, 4.x, and PowerChute Business Edition 10.x

Published date: 15 October 2020

Issue:
What files are needed to troubleshoot PowerChute Network Shutdown v3.1, 4.x and PowerChute Business Edition 10.x?

Product:
PowerChute Network Shutdown (PCNS) version 3.1 and 4.x
PowerChute Business Edition (PCBE) version 10.x

Environment:
All supported Windows and Linux OS

 
Cause:
Troubleshooting
 
Solution:

For PowerChute Network Shutdown:


Gather these files and send to Schneider Electric Technical Support
error.log, EventLog.txt, VirtualizationFileStore.properties, pcnsconfig.ini, javaVersionFile.log, debug.log
NOTE: VirtualizationFileStore.properties is only available with VMware (Nutanix, HPE SimpliVity, HyperFlex), Hyper-V, and Nutanix AHV configurations. 
 
On Windows the default path is
C:\Program files\APC\PowerChute\group1
 
On VMware vMA or APC Appliance the default path is
/opt/APC/PowerChute/group1

For PowerChute Business Edition:
Open the PowerChute Agent web interface and go to About, Create PowerChute Zip Archive.


  

NOTE: Other files may be needed at a later date and different files may be needed to troubleshoot installation issues.
 
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.