There is no filter on the condenser side on the ACSC; do I need to clean the coil?
Published date:
11 June 2020
Issue:
There is no filter on the condenser side; do I need to clean the coil?
Product line:
ACSC100, ACSC101
Environment:
InRow Cooling Cause:
Resolution:
Generally the condenser coil should not need cleaning. Fine dust may accumulate on the coil over time; however, this should not cause operational problems. The customer may elect to gently vacuum the coil annually.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.