Browse FAQs

NetBotz Appliances version 1 and 2 Operating Environments

Published date: 03 December 2019

Issue:

NetBotz version 1 and 2 Appliances Operating Environments

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2

Cause:

Opearting environment

Resolution:

The NetBotz Appliances and pods are designed for indoor use only.

The environmental operating conditions are as follows:

* Temperature: 35F to 120F (1.6C to 48.8C)
* Humidity: 10% to 90% non-condensing 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.