Browse FAQs



Netbotz Advanced View | Does NOT Support Radius, Active Directory or LDAP
NOTE: NetBotz Central, ISX Central, and StruxureWare Data Center Expert do support integrating with both Active Directory & OpenLDAP remote authentication server ...
NetBotz Web Client Does Not Load When Launched from the StruxureWare Data Center Expert UI to a NetBotz Appliance on the Private LAN
Users accessing StruxureWare Data Center Expert from the public LAN must use Advanced View to connect to a NetBotz appliance on the private LAN.
HTTP and HTTPS turned off by default on NetBotz 4.7
* use Advanced View and Data Center Expert to configure the appliance.
What types of Administrative system level alerts are produced by Data Center Expert?
Cancelled Backup - If a backup is in progress and someone cancels it through DCE User Interface.
Can Data Center Expert post to a syslog server?
... ) devices to post directly to syslog under the "Log" option in NetBotz Advanced View.
Data Center Expert | How do I upgrade my software version?
5) Select Install Update to start upgrading the server. 6) Monitor the progress of the update on the web interface of DCE.
Video: Data Center Expert | Backing up to a Windows Share
6) Select Share and then Done. 7) Select Advanced Sharing.
Data Center Expert | Obtaining an SNMP or Modbus DDF for discovery of third-party devices
NOTE: Try searching by the brand and also more advanced searches such as the family or exact model.
Data Center Expert | How do I enable SSL communication between StruxureWare and multiple Netbotz devices?
You can confirm these settings by accessing the Netbotz, through Advanced View, clicking on the Configuration Pane then the Infrastruxure Central icon located ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.