Temperature Sensor not detected on an AP9631 that was pre-installed in a Symmetra
Published date:
05 October 2018
Issue
An issue has been identified with AP9631's that come pre-installed in a single phase Symmetra unit - when connecting the temperature sensor to either UIO port, the NMC web UI will show either "Communication Loss", or will show a temperature sensor is connected, but not give any temperature reading:
Product Line
Network Management Card 2 - AP9631
Environment
AP9631 models that shipped preinstalled in a Symmetra - affected date range is 5A1641 and newer
Cause
These NMC's have an issue that does not allow them to see exactly how many UIO ports they have, which causes this behavior. Other UIO accessories, such as the AP9610 dry contact accessory, will also not work. The NMC will function as expected in all other ways, this issue only affects the UIO ports.
Resolution
This issue has been resolved in firmware with AOS v6.5.0+. Upgrading the firmware will immediately resolve the problem. The latest revision of firmware can be found on apc.com, or available via the Data Center Expert (DCE) catalog.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.