Browse FAQs



Why doesn't StruxureWare or ISX Manager's mass configuration feature update or show password credentials on APC Network Management Card devices?
Mass configurations of APC UPS ... devices done via ISX Manager or StruxureWare ... ... , ap9340, NetBotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... removed from the config .ini ... outside of the config .ini, This affects ISX Manager's ability to make mass configuration change of the ... . Because the ISX Manager takes one ... ... X, the config .ini ... blurb from a config .ini: The config .ini file could be manually configured outside of ISX Manager to include ...
How can I mass configure a Network Management Card (NMC) or NMC embedded product?
How can I mass configure a Network Management Card (NMC) or NMC embedded product? ... can I mass configure or configure multiple Network Management ... ... , ap9340, NetBotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... ... MasterSwitch 1/ 2 ) do not ... ... Card, mass configuration of those devices ... ... configuration file ( config .ini) ... ... Network Management Card 2 firmware v6 ... ... modified through the config .ini ... , these four settings will be disregarded ... ... keyword will not configure Output Voltage, ... ... I obtain a config .ini ... to retrieve the config .ini
Why can't I connect to my APC Network Management Card or embedded Network Management Card using a serial connection?
... , ap9340, Netbotz 200) ... Network Management Card 2 (NMC2) ... ... Network Management Card 2 include (but ... to): 2 G Metered/ ... Ensure you are connecting at the correct settings ... Please reference the product’s user manual for the default settings . ... by the user, a change to the configuration file, or a managing device like ISX Manager or StruxureWare Central. ... If you are having an issue connecting, try setting the baud rate to a different value:
Alert Actions for NetBotz Version 2 and 3 Appliances
... of the alert NetBotz 500, Camera ... speakers Call Web Services Alert Receiver Sends ... via the Web Services API to a remote system Properly configured web server running ... integrated with the NetBotz Web Services API
NetBotz | Configuring SeaLevel 450 Relay I/O Device
Environment: NetBotz version 2 and 3


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.