Browse FAQs



NetBotz 450/550/570 | Physical Description
NetBotz version 3 - Rack Monitor 450 (451)
Why is my Web/SNMP (ap9606) or Network Management Card 1, 2 or 3 not recognizing my UPS or device?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... ... Network Management Card 3 (NMC3) ... ... UI, v 3 .X. ... Device Type ... Single or three phase Smart-UPS, Galaxy 3500, Matrix UPS ... Three phase Symmetra UPS (except 250/500kva & PX2) Symmetra 3 Phase APP or sy3p ... Rack Power Distribution Units Rack Power Distribution APP or rpdu ... Lastly, if the firmware upgrade does not resolve the issue, there may be a problem with the Network Management Card or the UPS SmartSlot.
Network Management Card 2 (NMC2) - snmpv1/v3 walk beginning at .iso through .iso.org.dod.internet does not work properly
An snmpv1/v 3 walk beginning at .iso through .iso.org.dod.internet does not work properly with my Network Management Card 2 device. ... Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Certain Audio/Video Network Management Enabled products. ... SNMP v1/v 3 ... This issue is resolved in AOS 6.1.2 or higher.
Why are the red outlet LEDs always scrolling on Rack PDU models AP7855 or AP7867?
AP78XX Metered Rack PDU models, specifically ... The ( 3 ) load alarm thresholds are set incorrectly (Overload, Near Overload, and Low Load). You might find all three of these values are set to zero. Manually changing these values or resetting the unit to default settings should resolve this issue.
Common Rack Automatic Transfer Switch Scenarios and Questions
... article discusses common Rack Automatic Transfer Switch ... Rack Automatic Transfer Switches ... All Rack ATS models listed ... As the Rack Automatic Transfer Switches ... INFORMATION BULLETIN - Upgrading Rack ATS Firmware (AP77XX) - potential to permanently damage ATS during download. ... ATS firmware v3.5.7 and higher aims to resolve this issue and will help prevent the ATS from tripping the upstream circuit breakers. ... Revise the voltage transfer range from medium to wide, revise frequency deviation from +/-2 Hz to +/- 3 Hz on the ATS: ... Using the Rack ATS with a Generator
NetBotz v3 | How do I manage user credentials and login alerting?
... on a version 3 NetBotz appliance. NetBotz v 3 Wall Appliance: 355/356 (nbwl0355/6) & 455/456 (nbwl0455/6) NetBotz v 3 Rack Appliance: 450/451 (nbrk0450/1), 550 (nbrk0550), & 570 (nbrk0570) ... NetBotz v 3 (all versions) ... 3 ) Under Appliance Settings ... 3 ) Click OK ... 3 ) Chose a Privilege Set ... The user can also resolve alert conditions for thresholds that are configured with the Return-To-Normal Requires User Input setting in their Advanced Settings.
Video: How do I configure APC Network Management Card network settings?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP84XX ... AP89XX), Rack Automatic Transfer Switches ... ... Network Management Card 3 (NMC3) ... ... AP78XX or AP79XX Rack PDU, Environmental ... , there are three available options to ... ... Card 2/ 3 ... Card 2 and 3 based devices ( ... AP8XXX Next Gen Rack PDU (NMC2 ... ... have firmware version 3 .x. ... ... and has been resolved with AOS 6 ... ... program, any services using the COM ... ... the APC UPS service must be stopped ... Rack PDU (AP78XX ...
How To: Configuring an APC Network Management Card with popular email services such as Gmail, Yahoo!, Office 365, and Hotmail/Outlook.com
Popular email services such as Gmail ... to an external service ... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP86XX ... ... Network Management Card 3 (NMC3) ... ... using external mail services . ... an external email service such as Gmail ... ... is able to resolve the domain you ... ... for other mail services as well. 3 .) Navigate ... ... is able to resolve the domain you ... 3 .) Within ... This may be required for other mail services as well. ... The Network Management Card 2/ 3 (NMC2/NMC3) SMTP email Authentication Modes are explained below for reference.
Starting and Stopping PowerChute Network Shutdown on Windows Server Core
Solution : To start the PCNS service manually after it has been deliberately stopped, use either command below: ... "n" stands for the instance number, if only one instance was installed n=1 Each instance was it own number PCNS 2.2.3, 2.2.4 and 2.2.5 can have up to 3 instances. PCNS 3 .X and 4.X have 1 instance only so the entry is PCNS1.
What does the P N A mean on Stat section of my Network Management Card via the control console?
... Metered/Switched Rack PDUs (AP78XX ... AP79XX), Rack Automatic Transfer Switches ... ... Metered/Switched Rack PDUs (AP86XX ... ... X, v 3 .X. ... ... tells the NMC what type of unit it is ... If the issue is still not resolved , it may be necessary to reflash the firmware of the device. ipv6 (and N6) indicators are only visible on NMC2 based devices such as but not limited to ap9630, AP9631, AP9635, Rack PDU 2G - AP86XX, AP88XX, AP89XX, and Pro AV devices).


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.