Browse FAQs



How to configure NetBotz version 2 external sensors?
It’s always a good idea to test the sensors and cabling before fully deploying the solution on-site .
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
Definition of coverages as relates to the service level agreements offered by SE UPS & PDU On-Site Warranty Extension:
Adding External Batteries to an SU, SUM, SURT, SURTA, SURTD or SUA series Smart-UPS XL
For Information on which battery packs are compatible ... visit the product page for you UPS at http://www.apc.com
How can I check the battery voltage of my XBP48RM1U-LI / XBP48RM1U2-LI?
... -LI have battery management electronics in ... and when the battery pack is unplugged ... sensed and the battery pack output is ... ... cannot measure the battery voltage from the cable unlike the external battery packs with VRLA Batteries . To check the battery voltage either ... Choose Battery Scroll to page 5 to see the battery voltage (as the AC power is removed this will just show the battery voltage rather than the charging voltage) ... Measure the voltage on the Battery Pack Anderson socket with a voltmeter (as AC power is removed this will just show the battery voltage rather than the charging voltage)
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
... off using an external Maintenance Bypass Panel ... Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS ... This procedure is for a single UPS with an external maintenance bypass panel. Regardless of wall mount, or free standing, the external breakers have the same designation. ... Step 9: Set the battery circuit breaker(s) QF1 to Off Position. ... There is still stored energy in the capacitors, and batteries inside the UPS. Never remove any covers or panels.
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... ... than the low battery signal warning time ... ... than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... ... , the low battery signal time is ... UPS battery ... or replace the battery . ... , yet the batteries are consumable items ... As the batteries age, they ... ... of the low battery signal warning time, the battery charge LEDs will ... even if the battery is at 100 ...
My smx2200 or smx3000 series Smart-UPS displays "Battery Temperature Sensor Fault"
... UPS displays " Battery Temperature Sensor Fault ... ... UPS use Smart external battery backs to increase ... Each battery pack contains a ... ... If you connect external batteries , but fail ... connect the internal battery that is built ... issue with the Battery Temperature Sensor. ... exists at the battery temperature sensor" ... The battery temperature may show ... To correct this, please ensure the internal battery of the UPS is connected correctly. Please refer to the installation guide that accompanies the UPS or installation instructions from our website . ... After reseating the internal battery connecter, if the fault does not clear, please contact Technical Support to troubeshoot further.
APC Din Rail/Panel Mount UPS and External Batteries
... guide for for the APC Din Rail/Panel Mount UPS Battery Replacement specifies how to connect an External Battery to the UPS.
Where can I find BTU specs for Smart-UPS external battery packs?
Issue: Where can I find BTU specs for Smart-UPS external battery packs?
Why am I not able to establish communication with external batteries and my surt15k/20k UPS?
Issue: Cannot establish communications with external battery packs


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.