Browse FAQs



Can I change the individual batteries inside of a Smart-UPS replacement battery cartridge?
APC Replacement Battery Cartridges are intended to be replaced as a complete unit.
Used Battery Disposal Options
If you purchased an APC Replacement Battery Cartridge in the U ... return the old battery will be provided with the new Replacement Battery Cartridge .
Video: APC AV S Type Power Conditioner w/ Battery Back-up - Battery Replacement Procedure
Resolution: The following video details the process for removing and reinstalling the internal Replacement Battery Cartridge .
How do I recycle APC batteries in the US and Canada?
Pack the used battery in the packaging from the replacement battery cartridge and affix the return label.
Material Safety Data Sheets (MSDS) or Safety data Sheets (SDS) for Batteries Used in APC UPS Systems
In a few cases, Replacement Battery Cartridges (RBCs) containing High Power Lithium Ion Cell, Phosphate-Based are also used.
Why are the battery charge LEDs flashing on a Smart-UPS?
Battery Charge LED Bar ... ... than the low battery signal warning time ... ... than the low battery signal time, the battery charge graph LEDs ... ... Reset the low battery signal time to ... ... with the low battery signal warning time ... ... , then the battery bar graph LEDs ... ... setting the low battery signal warning time ... ... , the low battery signal time is ... UPS battery ... /www. apc .com/ ... ... the load or replace the battery . ... , yet the batteries are consumable items ... As the batteries age, they ...
Why should I use only genuine APC Replacement Battery Cartridge (RBC) in my APC UPS?
Using of a non- APC battery may result in lower runtime, damage the UPS, create hazardous conditions, or void safety certifications ...
Video: How to Select the Correct Replacement Battery Cartridge (RBC) for your UPS
To determine the correct Replacement Battery Cartridge to purchase for your APC UPS and to see other options available to you, use the
Can I mix old and new batteries in a Smart-UPS?
When replacing the battery cartridges in this APC Smart-UPS ... , the two battery modules for the ... and the four battery modules for the external battery pack should be ...
What are the basic troubleshooting steps for the APC AV J-Type J25B / J35B Power Conditioner and Battery Backup?
... steps for the APC AV J- ... Power Conditioner and Battery Backup ? APC AV J- ... Power Conditioner and Battery Backup ... find the your APC AV J- ... The internal battery is not connected ... Connect the battery . ... connect to a Battery Backup outlet. ... is operating on battery power, while ... Battery Backup outlets may ... ... equipment from the Battery Backup outlets and ... The battery was recently discharged due to a power outage and has not fully recharged. Charge the battery cartridge for 16 hours. The battery has reached the end of its useful life. Replace the battery .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.