Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
Network Management Card 660674/34003640SE; Ripple20 vulnerability status
Issue:
Ripple20 vulnerability status
Product line:
660674/34003640SE Network Management Card (NMC)
Environment:
660674/34003640SE Network Management Card (NMC)
Cause:
Information about the 66074 NMC and the Ripple20 vulnerability (Treck Inc.’s embedded TCP/IP stack).
Resolution:
The 66074 NMC does not use the Treck Inc.’s embedded TCP/IP stack for TCP/IP but use a inhouse TCP/IP stack developed by the NMC vendor. This NMC is not affected by this vulnerability.
Ripple20 vulnerability status
Product line:
660674/34003640SE Network Management Card (NMC)
Environment:
660674/34003640SE Network Management Card (NMC)
Cause:
Information about the 66074 NMC and the Ripple20 vulnerability (Treck Inc.’s embedded TCP/IP stack).
Resolution:
The 66074 NMC does not use the Treck Inc.’s embedded TCP/IP stack for TCP/IP but use a inhouse TCP/IP stack developed by the NMC vendor. This NMC is not affected by this vulnerability.
Did this answer your question?
Explore more
Explore more