Search FAQs
In the NetShelter WX 6U Vertical cabinet, must the included 2U UPS Mounting Bracket be used?
Issue:
It's unclear if the included 2U UPS Mounting Bracket must be used.
Product Line:
AR106V, AR106VI
Environment:
All versions and serial ranges.
Cause:
The AR106V/VI ships with a 2U UPS Mounting Bracket.
Resolution:
If the UPS is being installed into the cabinet prior to shipping, the 2U Mounting Bracket is required.
If the cabinet is not shipping with the UPS installed, then the UPS may be installed with its own mounting brackets.
It's unclear if the included 2U UPS Mounting Bracket must be used.
Product Line:
AR106V, AR106VI
Environment:
All versions and serial ranges.
Cause:
The AR106V/VI ships with a 2U UPS Mounting Bracket.
Resolution:
If the UPS is being installed into the cabinet prior to shipping, the 2U Mounting Bracket is required.
If the cabinet is not shipping with the UPS installed, then the UPS may be installed with its own mounting brackets.
Released for:APC Egypt
Explore more
Range:
Explore more
Range: