{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

NetBotz 450/550/570 | Physical Description

Issue:
Physical Description of the NetBotz 450/550/570.

Product Line:
NetBotz version 3
- Rack Monitor 450 (451)
- Rack Monitor 550 (551)
- Rack Monitor 570

Environment:
NetBotz v3 Rack Monitors (all firmware versions)

Resolution:

Physical Description



ItemDescription
1AC line inletProvides for the input power connection.
2Reset SwitchResets the appliance.
3Port activity LED.Flashes green with the RS485 port is receiving. Only available on the NBRK0570 appliance.
4RS485 portProvides for a Modbus connection. Only available on the NBRK0570 appliance.
510/100 Base-T Network PortProvides for a 10/100 Base-T network connection. Status and link LEDs indicate network traffic:
- Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address).
- Link LED: blinks to indicate network traffic (green = connected at 10 Mbps; orange = connected at 100 Mbps).
6Alert LEDIndicates the alert status of the system.  When more than one alert exists, the most severe will be indicated.
- Flashing once every eight seconds = Informational
- Flashing one very four seconds = Warning
- Flashing once every two seconds = Error
- Flashing once every second = Critical
- Flashing twice per second = Failure
7Voltage OutputProvides 12 VDC or 24 VDC (75 mA) to one connected device.
Relay Outputs ports 1,2Used for connecting relay-controlled external devices. Provides 24 VDC (100mA) each.
8Power LEDIndicates whether the unit is receiving power (green - receiving power; dark - not receiving power).
94-20 mA InputsProvides 24 VDC for connecting third-party sensors with an input current range from 4 to 20 mA.
10Sensor ports (4)Used for connecting APC by Schneider Electric sensors, third-party dry-contact sensors, and standard third-party 0-5 V sensors. Third-party dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304). Standard third-party 0-5 V sensors require the NetBotz 0-5 V Sensor Cable (NBES0305). NBRK0450/550 - 5/24 VDC 950mA). NBRK0570 - 5/24 VDC (200mA).
11Leak Rope portUsed for connecting a NetBotz Rope Leak Sensor (NBES0308).
12BeaconUsed for connecting an Alarm Beacon (AP9324).
13A-Link portUsed for cascading NetBotz sensor pods and temperature and humidity sensors with digital displays. Provides communications and power to the connected devices over standard CAT-5 cabling with straight-through wiring.
14Alert LEDSame as item 6 above.
15Power LEDIndicates whether the unit is receiving power (green - receiving power; dark - not receiving power).
16Console portUsed to connected a console to the appliance. Enable the USB-to-serial converter support (FTDI) in your operating system.
17USB Type A ports (2 or 4)Used to connect USB devices to the appliance. The NBRK0550 and NBRK0450 have two USB ports, while the NBRK0570 has four.
18Exhaust fanExhausts hot air from the NBRK0570. Not present on the NBRK0550 and NBRK0450.

The complete NetBotz 450/550/570 Installation and Configuration Manual can be found here.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.