{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}
{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

NetBotz 750 | Physical Description

Issue:
   Physical Description of the NetBotz 750

Product Line:
   NetBotz version 5
      - Rack Monitor 750

Environment:
   NetBotz v5.X

Resolution:

Physical Description



 
ItemDescription
1AC line inletInput power connection.
2Switched OutletProvides power to a device at a maximum of 10 A. Activates a connected device when configured events occur. (For example, a fan may be connected to this outlet, and the outlet may be configured to turn on when certain alarms are generated.)
3A-Link portsProvide communications and power to connected devices (sensor pods, rack access pods, and temperature/humidity sensors with digital displays) over standard CAT-5 cabling with straight-through wiring. For instructions to cascade devices, see the Installation and Quick Configuration Manual.
4Leak Rope portsUsed for connecting a NetBotz Leak Rope Sensor (NBES0308).
5Rack Access Ports*Ports for the door switch sensors (NBES0302 or NBES0303) and handle sensors (NBHN125 or NBHN1356).
6Universal Sensor portsUsed to connect APC by Schneider Electric sensors, third-party dry-contact sensors, and standard, third-party 0-5 V sensors. Third-party, dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304), and third party, 0-5 V sensors require the NetBotz 0-5 V sensor cable (NBES0305).
7Beacon PortUsed for connecting an Alarm Beacon (AP9324).
810/100/1000 Network PortProvides a connection to the network. Status and link Light-emitting Diodes (LEDs) indicate network traffic. See Link LED and Status LED for additional information.
9Private LANProvides a 10/100/1000 connection to a private local area network and 48 VDC to an attached device.
10Wireless Sensor CoordinatorUSB Port with Wireless NetBotz USB Coordinator (NBWC100U) installed. Used with wireless sensors.
11USB Type A PortsReserved for future use.
12Modbus RS485 PortReserved for future use.
13Voltage OutputProvides 12 VDC or 24 VDC (75 mA) to one connected device.
13Relay OutputUsed for connecting relay-controlled external devices. Relay Outputs can only be connected to Class 2 circuits.
144-20 mA InputsInputs for industry standard 4-20 mA sensors.
15Console PortProvides a serial connection to the appliance.
16Power LEDIlluminates when the unit is receiving power.
17Reset SwitchReboots the appliance.
18Exhaust fanExhausts hot air from the appliance.
*Note supported on firmware version 5.0.1. Update the firmware to access these features.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.