{}

Our Brands

Search FAQs

PowerChute Network Shutdown will not communicate with or drops communication with VMware ESXi 5.5 host

Issue:
PowerChute Network Shutdown will not communicate with or drops communication with VMware ESXi 5.5 host.
In the PowerChute error.log file the error Connection to ESXi Host could not be made.java.rmi.RemoteException: VI SDK invoke exception:javax.net.ssl.SSLHandshakeException: Remote host closed connection during handshake is recorded.

Product Line:
PowerChute Network Shutdown v4.0, v4.1, v4.2

Environment:
Vmware ESXi 5.5 host

Cause:
VMware service patch

Solution:
Install the latest VMware patch ESXi550-201612001

APC Egypt

Did this answer your question?

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.