{}

Our Brands

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

What is the definition of the shutdown types in PowerChute Business Edition?

Issue:
Need to know the different shutdown types in PowerChute Business Edition.

Product Line:
PowerChute Business Edition

Environment:
All supported Windows OS

Cause:
Informational

Solution:
Depending on the UPS model and the version of PowerChute the options are

Shutdown
Shutdown and off
Hibernate


Both the Shut Down options shut down your operating system. Shut Down and Off also turns off your computer. If your computer BIOS power management setting is set to [Last State], the computer does not turn on again automatically when the UPS resumes the supply of power. If your computer BIOS power management setting is set to [Always On], the computer does turn on again. For assistance with the system BIOS see Computer will not automatically reboot after UPS has shutdown and restarted
If the OS is Windows 2003, 2008, or 2012 see After a graceful shutdown by PowerChute, Windows 2003, 2008, or 2012 system fails to turn on when utility power is restored.

NOTE: Hibernation must be enabled before it can be selected and it is not available in PowerChute Business Edition Agent versions 9.1, 9.1.1, 9.2, 9.2.1, 9.5, 10.x
Warning: With hibernation as your shutdown type, PowerChute scheduled shutdown operations do not perform normally. You should not schedule shutdowns when hibernation is in use.

Did this answer your question?

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.