{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Data Center Operation | Server is running low of storage space.

Issue:
StruxureWare Operation server is running low of storage space.

Product Line:
StruxureWare Data Center Operation (DCO)

Environment:
StruxureWare Data Center Operation (All Versions)

Cause:
Server does not have enough storage space to either run another backup or Operation services will not start because of backup or old data and jobs.

Resolution:

The best option would be to increase the storage size for the virtual machine hard drives. To temporally increase available space on the hard drives, Operation has a built-in service to purge old data, files, and jobs. Console into the server and run the following command:

sudo service operations purge

It is also recommended that old backups are manually moved or deleted from the /data/backup directory. To manually delete old backups navigate to /data/backup from the root directory. Then run the following command.

rm <filename>

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.