{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Did this answer your question?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

PowerChute Network Shutdown fails to run command file on HP-UX

Issue:
Run command file fails to work when an event is triggered.

Product:
PowerChute Network Shutdown versions 3.0.1, 3.1

Environment:
HP-UX 11iv3

Cause:
Install PowerChute and configure in Single mode. Configure command file for on battery in the configure event page. Also configure command file in the shutdown settings page. Generate on battery event.

Expected Result: Command file should run

Actual Result: Failed to run the command file


Resolution:
Upgrade to PowerChute Network Shutdown version 4.x

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.