{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Did this answer your question?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
BMS AP9921X-AP9922; Environment Alarms
Issue:
BMS AP9921X-AP9922; Environment Alarms
Product line:
Battery Management System (BMS) AP9921X & AP9922
Environment:
All models, all serial numbers
Cause:
Critical Alarms
High Ambient Temperature:
The air temperature in the battery string environment is above the configured threshold. Default high threshold: 95.0°F (35°C) Check temperature control and ventilation systems in the room, and check for overheated batteries (usually caused by overcharging). NOTE: Lead-Acid batteries provide optimum output and longevity at 77°F. An uncorrected high temperature can significantly shorten the life of the battery string.
Warning Alarms
Low Ambient Temperature:
The air temperature in the battery string environment is below the configured threshold. Default low threshold: 50.0°F (10°C) Check temperature control and ventilation systems in the room. NOTE: Lead-Acid batteries provide optimum output and longevity at 77°F. An uncorrected low temperature can prevent the battery from providing adequate power to the UPS, and will cause the UPS to drop the load prematurely.
Input Contacts:
Activation of input contacts triggers an alarm. Check the status of the external monitoring device that sent the input signal.
Resolution:
Correct the cause of the failure symptom, alarm.
Can't find what you are looking for?
Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.