{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Did this answer your question?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Alert Actions for NetBotz Version 2 and 3 Appliances

Issue:
Alert Actions for NetBotz Version 2 and 3 Appliances

Product Line:
Netbotz

Environment:
NetBotz Version 2 and 3 appliances

Cause:
The NetBotz Version 2 Appliances (320, 420, 500) support a variety of alert actions. Version 3 4xx and 5xx NetBotz also support these alerts based on configuration / connections. Some of these alert actions are only applicable if the required hardware and/or software is available. The following table defines the available alert actions and required hardware.

Resolution:

Alert ActionResultsPrerequisites
Send EmailSends an email via SMTP to one or more target recipientsnone
Send Short Message EmailSends a custom formatted email via SMTP to one or more target recipientsnone
Send SMS MessageSends an SMS text message via GSM service providerGPRS / GSM Wireless Adapter
Send SNMP V1 TrapSends an SNMP version 1 trap to configured targetsnone
Send HTTP POSTSends standard (all) alert information formatted in XML to a web server in the form of an HTTP POSTProperly configured web server and application code
Send Custom HTTP GetSends customized alert information to a web server in the form of an HTTP GETProperly configured web server and application code
Send Data to FTP ServerSends standard alert data formatted in XML to an FTP server.Properly configured FTP server
Send Custom Text File to FTP ServerSends custom alert text file to an FTP serverProperly configured FTP server
Set Switch Output StateSets the state of an device switchSupported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip
Activate Button StateActivates a push button defined on an output deviceSupported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip
Play Audio AlertPlays or speaks the text of the alertNetBotz 500, Camera Pod 120 and attached external, power speakers
Call Web Services Alert ReceiverSends customer alert information via the Web Services API to a remote systemProperly configured web server running custom application code integrated with the NetBotz Web Services API


Note: Refer to the NetBotz documentation for configuring the prerequisite hardware and software.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.