{}

Our Brands

{"support":{"yesButton":"yes","noButton":"no","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

How to configure NetBotz version 2 external sensors?

Issue:
Netbotz External Sensor Installation Tips

Product Line:
Netbotz

Environment:
NetBotz 2.x

Cause:
Configuration tips.

Resolution:

Adding sensors that connect to the external sensor ports require configuration before they will function. Follow these basic guidelines when adding sensors to the external sensor ports:
  • Physically connect the add-on sensor using and noting the external sensor port(s)
  • Under “Configuration” in the Advanced View, click on “Sensor Pods”. Select the appropriate Sensor Pod where you attached the sensor
  • Click “External Ports” and select the appropriate sensor and the port that it’s plugged into, then name it appropriately
  • Once that’s done, you can then select the “Sensors” button and edit the thresholds for that device accordingly
  • It’s always a good idea to test the sensors and cabling before fully deploying the solution on-site.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.