Search FAQs
{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
What is the Smart-UPS On-Line surge and spike test data?
Issue:
What is the Smart-UPS On-Line surge and spike test data?
Product Line:
Smart-UPS
Environment:
All models, All Serial Numbers
Cause:
Product Information
Resolution:
The Smart-UPS On-Line products have been tested to levels that exceed IEC standards for voltage spikes, voltage surges, and voltage swings. Below is the IEC standard level as well as the Smart-UPS On-Line test level.
Voltage Spikes
IEC standard (level): IEC 61000-4-4 (1000 volts)
SUOL test level: 4000 volts
SUOL test result: Passed
Voltage Surges
IEC standard (level): IEC 61000-4-5 (1000 volts)
SUOL test level: 6000 volts
SUOL test result: Passed
Voltage Swings
Within the ONLINE range, the SUOL will draw power from the ac-input source, charge the batteries, and regulate the output voltage to within 1% of nominal (typical): This range is dependent on UPS load as follows:
* 160Vac - 280Vac if load is above 50% of UPS rating
* 100Vac - 280Vac if load is 50% of UPS rating or below
Outside the ONLINE range, the UPS will transfer to battery backup power and continue to regulate the output voltage.
Did this answer your question?
Explore more
Range:
Explore more
Range: