Browse FAQs



How to navigate through an Network Air FM unit display
Operation . ... MultiCool® ( chilled water) and ... Indicates the humidity control method. ... can control the humidity based on the relative humidity (RH • Relative humidity (RH ... and the return humidity value. ... near the environmental sensors , and is ... temperature and relative humidity of the room ... ... , then the cooling setpoint is used ... humidity is 40% ... ... when the remote sensor readings are used ... ... avoid over- cooling while dehumidifying. ... the modes ( cooling , reheat, ... ... System cannot begin operation until this delay ... ... It allows the sensors to obtain an ... Sensor setup
NetBotz 250 | Inaccurate Data Logs (prior to v6.4.6 firmware)
Device > Wired Sensor > Temperature & Humidity ) now report the same value if updated at the same time.
How does a chilled water actuator work on an acrc301h to control dew point after a power loss?
Upon restart, the fans start first to allow the sensors some time to recognize the air temperature and humidity as well as the fluid ...
Data Center Expert | Determining Sensor Baselines (High/Low)
... , the temperature may get hotter on the weekend if you depend on HVAC to cool the room and the A/C is turned ...
NetBotz 700 Series | Wireless Network (Coordinator / Sensors)
... manage a wireless sensor network. NetBotz Wireless Sensors ... Connecting the Wireless Sensor Network The wireless sensor network is made ... ... Appliance) collects data from the wireless sensor network and generates alerts based on sensor readings. It reports data from the sensors on the network ... Each wireless sensors network must have ... ... of the wireless sensor network. Routers pass information between themselves and ... In a data center environment where obstructions ... are recommended if sensors are more than ... ... attached and internal sensors and send data back to the ... INFO ! ... (Routers/ Sensors )
How to set points and sensor offsets on a Uniflair High Capacity unit with Touch Screen Display
How to set points and sensor offsets on a Uniflair High Capacity unit with Touch Screen Display. ... • Humidification Setpoint Relative Humidity : ... • Humidification Proportional Band Relative Humidity : ... • Dehumidification Setpoint Relative Humidity : ... • Dehumidification Proportional Band Relative Humidity : ... • Return Air Temperature Sensor Offset: ... • Supply Air Temperature Sensor Offset: ... • Return Air Relative Humidity Sensor Offset: ... • Circuit Entering Chilled Water Temperature Sensor Offset: - ... • Circuit Leaving Chilled Water Temperature Sensor Offset: ... • Outdoor Temperature Sensor Offset: Delta ... • Hot Water (Reheat) Temperature Sensor Offset: Delta
What sensors are supported by the NetBotz Wireless Sensor Pod 180 (nbpd0180) ?
... The NetBotz Wireless Sensor Pod 180 ( ... supports the following sensors : Sensor Name ... NetBotz Door Switch Sensor for APC Racks ... NetBotz Door Switch Sensor for APC Racks ... NetBotz Door Switch Sensor for Third Party ... NetBotz Door Switch Sensor for Rooms or ... nbes0302 APC Temperature Sensor - 13 ft ... APC Temperature & Humidity Sensor - 13 ft ... Sensor - 32 in ... : Only the sensors listed above are compatible with the nbpd0180. Other sensors will not function and will damage the device. For more information , please see the nbpd0180 Installation Guide & NetBotz Wireless Sensor Setup Addendum below.
Which accessories/environmental sensors are compatible with my APC Network Management Card (or devices with embedded Network Management Cards)?
... accessories or environmental sensors are compatible with ... General compatibility information relating to supported ... to the " Sensor " or " ... ... refer to NetBotz sensor compatibility information . Accessories/ Sensors Supported AP9335T Temperature Sensor ... AP9335TH Temperature/ Humidity Sensor AP9335T Temperature Sensor ... AP9335TH Temperature/ Humidity Sensor AP9335T Temperature Sensor ... AP9335TH Temperature and Humidity Sensor AP9335T Temperature Sensor ... AP9335TH Temperature/ Humidity Sensor AP9335T Temperature Sensor ... AP9335TH Temperature/ Humidity Sensor ... Party) r170 Sensor Tag, requires ... ... A, no Sensor port(s ... ... A, no Sensor port(s ... ... AP9619 1/ Sensor Any N/A, no Sensor port(s) available ... N/A, no Sensor port(s) available
What are your Cooling Product Energy efficiency rating (EER)?
... to calculate your Cooling Product Energy efficiency ... ... of a particular cooling device is the ... cooling (in Btu ... ... 50% relative humidity . ... COP of a cooling device is unit ... less: the cooling load and the ... In regards to Schneider Electric's cooling products this can be calculated from the Technical Data Manuals, or Technical Data Specifications. ... = rated cooling capacity output (kW)/ cooling input power (kW)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.