Technical FAQs

Ask a Question

NetBotz v3 | Cannot create new dialog class within Advanced View

Issue:
In Advanced View an error can occur when accessing the SNMP menu, "Cannot create new dialog class: com.netbotz.plugins.config.SNMPEditPanel"

Product Line:
NetBotz v3 (355, 450, 455, 550, & 570)

Environment:
NetBotz v3 (all firmware version)
Advanced View (all versions)

Cause:
An issue within the local configuration file may cause this error to appear.  Deleting the local client configuration files should resolve the issue.

Resolution:

Delete the user configuration file that is usually located in your users directory:
C:\Users\"username"\.netbotz

NOTE: This file contains user configuration settings for the Advanced View application.
Was this helpful?
What can we do to improve the information ?