Consultar las preguntas frecuentes



What type of battery could I use with the Galaxy VS UPS?
Galaxy VS, 3 Phase UPS , Uninterrupted Power Supply, 10 kVA , 15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ... use with the Galaxy VS UPS ?, battery ...
Video: How can the Galaxy VS reduce my energy bill?
Galaxy VS, 3 Phase UPS , Uninterrupted Power Supply, 10 kVA , 15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ...
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
How to take the Single Galaxy 5000 UPS from normal operation to total power off ... Galaxy 5000, Galaxy 5500 Due to site maintenance, ... request come in for assistance with Powering Down the Galaxy 5000 UPS The instructions to power down the UPS are available on ... ... This procedure is for a single UPS with an external ... Step 1 : Touch any ... on the display to wake it up ... ... 3: Scroll to “Maintenance” ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to transfer the load to the Static Bypass ...
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power off to normal on- ... Galaxy 5000, Galaxy 5500 For various reasons, the Galaxy 5000 may be ... ... guide illustrates how to restore it to normal operation. ... This is not for commissioning a new UPS . ... of a new UPS must be performed ... trained and qualified service representative. How to restore the Galaxy 5000 UPS from total power off to normal operation. ... This procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On
What are the factors that affect Battery Rated Service Life?
... affect Battery Rated Service Life? ... design life of 5 years, 8 years, 10 years, etc ... ... That is their Service Life Symmetra, Galaxy , EPS, Smart UPS , Battery ... that affect battery service life. 1 )Design Life ... regimen that has to be followed very accurately in order to achieve the Design ... ... This specification is for the internal temperature ... , and not for the ambient room ... ... cabinet can be 10 F warmer, ... ... life is halved for every 10 °C above ... ... is specifically designed to be installed
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
Wiring information for egx100 to any 66061- ... ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW Wiring information for egx100 to any 66061- ... ... card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is connected to the enclosure but ... ... card is RS232 for configuration. ... must be wired to . ... IP address needs to be configured at ... One is down ( ...
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 Due to site maintenance, ... request come in for assistance with Powering Down the Galaxy 5000 UPS The instructions to power down the UPS are available on ... ... This procedure is for a single UPS without an external ... Step 1 : Touch any ... on the display to wake it up ... ... 3: Scroll to “Maintenance” ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to transfer the load to the Static Bypass ... ... protected by the UPS .
Video: How to place Galaxy VM UPS into Maintenance Bypass
Cause: The UPS must be transitioned into maintenance bypass mode for certain types of service or other maintenance to the system.
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
Smart- UPS VT- Galaxy 3500; Bypass ... Smart- UPS VT- Galaxy 3500-ais3000 ... of acceptable range for bypass operation. ... occurs when the UPS is online, ... , the UPS should not allow you to command the UPS to bypass. If the UPS allows you to enter Static Bypass ... alarms are displayed for 20> seconds ... the input voltage to provide acceptable voltage ... ... Input frequency range for the PFC is ... ... window, the UPS should be in ... For 60 Hz systems ... ... - 0, 1 % For 50 Hz systems ...
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel) is set to synchronize time.


Resultados 1 - 10 de 69

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.