Consultar las preguntas frecuentes



No power output from the Matrix-UPS L14-30 or 5-15 receptacles (mx3000/5000)
Issue Matrix-UPS is not providing any output power to the receptacles on the rear of the UPS .
How do I cold start the Matrix-UPS?
When the dual pole input circuit breaker is moved to the ON position, this action turns the Matrix-UPS logic on.
Matrix-UPS frequently asked questions regarding installation, operation, and standards
... questions about the Matrix UPS ? Matrix UPS ... use of a Matrix UPS . ... of the APC Matrix UPS . 1. Matrix-UPS should be set ... ... input voltage to Matrix-UPS . ... 240vac input, Matrix-UPS Input Select Tap ... ... 3. Set Matrix-UPS EU (Electronics ... on top of Matrix-UPS IU (Isolation ... ... on top of Matrix-UPS or by its ... 5 . Hook Anderson ... ... " marking of first SmartCell. ... the rear of Matrix-UPS IU to " ...
Matrix-UPS emits a chirping sound after being on-battery or running a self-test
Matrix-UPS emits a chip ... completed or the UPS has been on ... Matrix-UPS ... If a SmartCell battery pack fails a UPS On-Battery Self-test (either scheduled or through UPS start -up), the Matrix-UPS will emit chirps for an interval of one minute to warn of a Replace Battery condition. The Matrix-UPS will emit the chirping sound once every five hours and will continue this chirp cycle until completion of a successful On-Battery Self-test.
Matrix-UPS Displays Overload on Display Panel
Issue Matrix-UPS displays an overload on the front display or via the network management card.
What are the Matrix-UPS operating temperature limitations?
The Matrix-UPS will operate within all standard specification ratings in a surrounding (or environmental) temperature range of 0°C to ...
Does the Matrix-UPS charge the batteries in Bypass mode?
The Matrix-UPS does not charge its batteries in bypass mode.
Does the Matrix-UPS have PDU options to provide for other output receptacle needs?
APC by Schneider Electric used to have several optional PDUs for use with the Matrix-UPS to provide greater flexibility of electrical connections.


Resultados 1 - 10 de 31

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.