Consultar las preguntas frecuentes



Can the ar7708 Hot Air Recirculation Prevention Kit be used in a NetShelter SX Networking cabinet?
The ar7708 Hot Air Recirculation Prevention Kit is designed for use with the standard NetShelter SX cabinets, not the Networking cabinets.
Do the Cisco Nexus 7700 series switches require a side airflow duct kit?
Customers ask if the Nexus 7700 series also requires side airflow duct kits . ... NetShelter SX ... Duct kits are used to help the switches cool efficiently and prevent hot air recirculation .
Does APC offer a side airflow duct kit for the Cisco Nexus 7009, 7000 9-slot switch?
Cisco Nexus 7009 requires a side airflow duct kit when installed in a NetShelter cabinet. ... NetShelter SX ... This side airflow duct kit is designed specifically to allow the Cisco Nexus 7009 to install into the NetShelter cabinet and draw the additional air required to cool properly. ... It also helps block hot air from recirculating to the front of the cabinet.
When finger-style vertical cable managers are used in a 750mm wide NetShelter cabinet, is it possible to also block off the cable pass-thru openings in the mounting rails?
Using the finger-style vertical cable managers inside a NetShelter cabinet, designers need to know how to block hot air from recirculating through the rails. ... NetShelter SX ... If left open, hot air can recirculate through these holes. ... When there are finger style cable managers installed inside the 750mm wide NetShelter cabinet, AR7714 must be used to prevent hot air recirculation .
How is the rackmount U-space of a NetShelter cabinet or rack identified?
NetShelter SX ... Incorrect placement of equipment can create airflow problems, like hot air recirculation .
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
NetShelter SX Wide cabinets, vertical cable management and horizontal troughs. ... All 750mm wide NetShelter SX cabinets: ar7580a, AR7585, AR7588, ar8008blk, ar8016ablk; all serial numbers. ... A customer wants to use both vertical finger-style vertical cable managers and horizontal cable troughs on the mounting rails of a 750mm wide NetShelter SX cabinet. ... Additionally, you may also use the roof brush strips AR7714 (5 per pack) to close off the holes in the cable managers and prevent hot air recirculation .
Is there a baying kit or bracket to connect a NetShelter SX to a VX?
Resolution: There are no baying brackets or kit which allow a SX cabinet to bay to a VX cabinet.
Is there a Recessed Rail Kit available for the 45U NetShelter SX cabinets?
Resolution: There are currently no recessed rail kits for the NetShelter SX 45U cabinets.
What effect, if any, do the magnetic panels of the Vertical Exhaust Duct Kits have on high speed network cables?
Issue: The NetShelter SX Vertical Exhaust Duct Kits include magnetic panels.
Is there a kit available to convert from a NetShelter SX cabinet to a NetShelter SX Networking cabinet?
There is currently no kit available to convert a NetShelter SX cabinet into a NetShelter SX Networking cabinet. The rails are not sold separately.


Resultados 1 - 10 de 69

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.