Consulter la FAQ

NetBotz 750 | Network Port Light Indicators

Date de publication : 22 July 2020

Issue:
Description of the Network Port lights (Link/Status) on NetBotz version 5.

Product Line:
NetBotz 700 Series
      - Rack Monitor 750 (NBRK0750)

Environment:
   NetBotz v5.X

Resolution:

Link (10/100/1000) LED
The LED on the right of any network port indicates the network status.
 
Condition Description
Off One or more of the following situations exist:
  • The Appliance is not receiving input power.
  • The cable that connects the appliance to the network is disconnected or not functioning properly.
  • The appliance is turned off or not operating correctly. It may need to be repaired or replaced. Contact Customer Support at www.apc.com/support.
Solid Green The appliance is connected to a network operating at 100 Megabits (Mb) per second or 1000 Mb/1 Gigabit (Gb) per second.
Solid Orange The appliance is connected to a network operating at 10 Mb per second.
Flashing Green The appliance is receiving or transmitting data packets at 1 Gb per second.
Flashing Orange The appliance is receiving or transmitting data packets at 10 Mb or 100 Mb per second.

Status LED
The LED on the left side of any network port indicates the status of the appliance.
 
Condition Description
Off One of the following situations exists:
  • The appliance is not receiving input power.
  • The appliance is not operating properly. It may need to be repaired or replaced. Contact Customer Support at www.apc.com/support.
Alternately Flashing Green and Amber The appliance is waiting for a DHCP server to assign a valid IP address.
Solid green The appliance is on and has a valid IP address.

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.