Consulter la FAQ

NetBotz 750 | How do I connect serially?

Date de publication : 16 July 2020

Issue:
How do I serially connect to the NetBotz 750?

Product Line:
NetBotz version 5.X

Environment:
NetBotz v5.X

Cause:
Serial parameters and drivers are required to establish a serial connection between a computer and the NetBotz appliance.

Resolution:

The NetBotz 750 uses the following serial parameters:
   - Baud Rate: 115200
   - Data Bits: 8
   - Parity: None
   - Stop Bits: 1
   - Flow Control: None

To log in and configure the 750 with an IP, you will need to log in with root as the user and you will be prompted for a password.

If you connect your NetBotz 750 to your computer and do not see it show up as a serial port (unknown device), you need to download the driver:

Serial port driver - Silcon Labs CP2103
https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers

Cela vous a-t-il aidé ?

Que pouvons-nous faire pour améliorer l'information ?

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.