Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... /AP9617/ 8 /9 installed Manual - Secure CoPy (SCP ... 8 . Wait for ... ... no parity, 8 data bits, ... 8 . Select option ... ... 57600 bps, 8 data bits, ... 8 . Type reset ... ... 57600 bps, 8 data bits, ... ... window on a PC which is connected ... 8 . Repeat Steps 3 - 8 again for the ... 2. Open an MS-DOS command prompt window on a PC which is connected to the network. ... Manual (via Secure CoPy) - Network Management Card 1, 2, and 3 ... Manual (via Secure CoPy) - Network Management Card 3