Consulter la FAQ



What type of battery could I use with the Galaxy VS UPS?
Galaxy VS , 3 Phase UPS , Uninterrupted Power Supply, 10 kVA , 15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ... use with the Galaxy VS UPS ?, battery ...
Video: How can the Galaxy VS reduce my energy bill?
Galaxy VS , 3 Phase UPS , Uninterrupted Power Supply, 10 kVA , 15 kVA ,20 kVA , 20 kVA ,30 kVA ,40kva, ...
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
How to take the Single Galaxy 5000 UPS from normal operation to total power off ... Galaxy 5000, Galaxy 5500 Due to site maintenance, ... request come in for assistance with Powering Down the Galaxy 5000 UPS The instructions to power down the UPS are available on ... ... This procedure is for a single UPS with an external ... Step 1 : Touch any ... on the display to wake it up ... ... 3: Scroll to “Maintenance” ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to transfer the load to the Static Bypass ...
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel) is set to synchronize time.
Does the NTP need to be configured on all NMCs for all parallel Galaxy VS?
Resolution: Ensure that only one network management interface in the entire UPS system ( single or parallel) is set to synchronize time.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power off to normal on- ... Galaxy 5000, Galaxy 5500 For various reasons, the Galaxy 5000 may be ... ... guide illustrates how to restore it to normal operation. ... This is not for commissioning a new UPS . ... of a new UPS must be performed ... How to restore the Galaxy 5000 UPS from total power off to normal operation. ... This procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On ... end of the UPS initialization with PFC ...
Galaxy VS; Why is FTP being logged in the event log but no external cause for logging FTP found?
Some UPS to NMC communications like Waveform generation are being logged by the NMC. FTP events should be communications between NMC and external applications ...
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
Wiring information for egx100 to any 66061- ... ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW Wiring information for egx100 to any 66061- ... ... card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is connected to the enclosure but ... ... card is RS232 for configuration. ... must be wired to . ... IP address needs to be configured at ... One is down ( ...
Which modular batteries can be used with the Galaxy VS All in One (AIO) model?
... used in the Galaxy VS All in One (AIO) ... Galaxy VS All in One Galaxy VS AIO model has the option to work with modular ... ... batteries are available for installation in the ... external battery frames for extended run time ... Wide Frame UPS , Tall Frame UPS , and Modular ... UPS will stay in ... Narrow Frame UPS : UPS will stay in ... UPS will stay in ... ... is not possible to program different batteries into a UPS . GVSBTU Galaxy VS 7 Ah Smart Modular Battery ( single module) GVSBT4 Galaxy VS 7 Ah Smart ...
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 Due to site maintenance, ... request come in for assistance with Powering Down the Galaxy 5000 UPS The instructions to power down the UPS are available on ... ... This procedure is for a single UPS without an external ... Step 1 : Touch any ... on the display to wake it up ... ... 3: Scroll to “Maintenance” ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to transfer the load to the Static Bypass ... ... protected by the UPS .


Résultats 1 - 10 de 67

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.