What are some features I need to be aware of while manipulating the config.ini file of a APC Network Management Card?
Product Line ... v3. X . X and higher ... downloaded using command line FTP or SCP ... ... options on the network card or unit it ... ... back on a network card , the override ... under the UPS device settings section ... specific section with UPS values and UPSOverride ... ... =APC_ UPS ... number of the UPS in which the ... On newer generation Micro-link UPS devices, such as SMX, SMT, SRT, and SURTD the following keywords in config.ini are protected by UPSOverride: ... For more details on UPS "generations," refer to .