Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
... to download and install the client application ... Resolution : ... discusses downloading and installing the Desktop Client ... ... PC with a 1 -GHz or ... 7, Windows 8 , or Windows ... At least 1 GB of RAM Screen resolution should be set ... at least 1024 x 768. 1 ) Open the ... 5 ) Run the downloaded execuatble file and follow the on-screen instructions. 6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation ) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.