Consulter la FAQ



Where can I find Hazardous Materials Quantities for C&D Technologies batteries used in MGE EPS, Galaxy and galaxy PW products?
EPS 6000, EPS 7000 , EPS 8000, Galaxy PW, Galaxy 5000, Galaxy 4000 ... Resolution : ... G5K 40kva with one string of UPS12-490fr will have 36 batteries, 100% run time 61 min.
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... support Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300/ 7000 , Galaxy 5000/5500, etc ...
Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
... PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250- 500 kva , SUVT, ... , ais3000, Galaxy VM
MGE Galaxy 5000 Installation, Technical Specs and Operation Manuals
... com/shop/us/en/products/MGE- Galaxy -5000-100- kVA /P-g5tups100
How do I properly install/uninstall my SmartSlot accessory card into my UPS?
All Symmetra 1 & 3 phase, Smart UPS VT, Galaxy 3500, and other 3 phase product lines
Galaxy 5000; Modbus Q1 Input Breaker status does not change state
Modbus Q1 Input Breaker status does not change state Resolution :
Which modular batteries can be used with the Galaxy VS All in One (AIO) model?
The modular batteries are available for installation in the main frame as well as external battery frames for extended run time.
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Due to site maintenance, inclement weather, and other conditions, request come in for assistance with Powering Down the Galaxy 5000 UPS Resolution :
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Resolution : Ensure that only one network management interface in the entire UPS system (single or parallel) is set to synchronize time.
Galaxy VM Seismic Certification and Anchoring Requirements.
Galaxy VM Seismic Certification ... Galaxy VM ... for documentation regarding Galaxy VM Seismic Certification ... Installation shall comply with ... Installation to be completed ... ... details prior to installation and site preparation ... Resolution : Galaxy VM Product Home ... ... -ups/ galaxy -vm/ ... Galaxy VM- 2012 ... Galaxy VM OSHPD pre ... ... -SA- Galaxy VM Typical Seismic ... ... 9GN8T9_R 1 _EN/ Galaxy VM Installation Manual: ... Galaxy VM Seismic Anchoring Document: BYSN-9GN8T9_R 1 _EN Galaxy VM Seismic Certification Document: COCR-9X4HHB_R0_EN


Résultats 1 - 10 de 64

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.