Consulter la FAQ



APC Schneider Cooling Unit Identification
Resolution : Capacity KW X = No Reheat ... X =No Humidifier ... FM- CW Capacity KW X = No Reheat ... X = No Humidifier ... Capacity KW X = No Reheat ... X = No Humidifier ... Capacity KW X = No Reheat ... X = No Humidifier ... Capacity KW ... AFX 018 ( 5 T) X = No Reheat ... X = No Humidifier ... ... -XXX- X Capacity KW 27 ( 8 T) ... -XXX- X -XX 28 (3 Bay ... ... -XXX- X -XX- X Capacity KW 017 ( 5 T) A ...
ACSC1XX Spare Parts List
Install , Repair. Resolution : ... BRACKET SCREW M 5 X 12 FLT UCUT PHIL M 5 X 12 BLK ( ... ... MTL PPR 400v 5 % 40uf RD ... ... .13" X .13" X .13" ... .19" X .19" X .19" ... , 3/ 8 " ODF ( ... ... ASSY - 17 KW IR ... FITTING 1/ 8 " BARB 10 ... ... FITTING 1/ 8 " BARB TEE ... ... DRIER 3/ 8 "ODF SOLDER ... FOOT LEVELING m10 X 51 L X 28 OD NYLOK
“Failed dependency error on terminal” during PowerChute Business Edition 8.0.1, 9.0.x, 9.1.x and 9.2.x installation on Red Hat Enterprise Linux 6.x, 7.x and Oracle Linux 7.3
The installation requires 32- ... ... .1. x , ... versions 6. x and 7. x ... x64 Operating System installation . ... "glibc- x .xx- x .xx. ... ... -freebl- x .xx. x - x .xxx. ... ... * glibc- x .xx- x .xx. ... -freebl- x .xx. x - x .xxx. ... (Replace x with the relevant ... ... -freebl- x .xx. x - x . x .xxx. ... rpm is not installed
Spare parts list for ACRD1XX, and ACRD2XX
Resolution : ... DOOR ASSY 10 KW - SPARE PART ... ... 380.0 5 .450 69 ... w0p2570 CRAC 8 X 2 FORM- ... ... " STRAIGHT C X C - SPARE ... 3/ 8 " ODF - ... 1/2"ODM X 5 / 8 " ODF EXTENDED, r410a 3 TON - SPARE PART 0.656 160.0 160.0 160.0 0.561 160.0 110.0 85
ACRP1XX, ACRD5XX, ACRP5XX, and ACRC5XX Parts List
Resolution : ... CABLE ASSY ACRP CW MAIN CTRL w0w4760 ... acrp5xx 208v ( CW ... acrp5xx 480v ( CW ... p30a to P 5 & P6 ... - acrp5xx ( CW ... p30a to P 5 & P6 ... /PROBE EMU 8 FT - SPARE ... /PROBE EMU 8 FT ASSY ( ... ... for ACRPxxx ( CW AND DX ... FAN acrp5xx ( CW ) ... Reheat acrp5xx ( CW ) ... for acrp5xx ( CW ) ... Breaker 2P 5 A 240v ... Breaker 2P 5 A 480v ... Breaker 3P 5 A 240v ... Breaker 3P 5 A 480v ... Breaker 3P 8 A 480v
EcoBreeze Variable Speed Drive Technical Spec’s
Resolution : ... - 15kw - 28 .5kva ... 240 V - 5 ... 5 % ... Hz (- 5 ... 5 %) Motor power kW 15 kW ... AI2, AI3 8 ms for analog ... ... AOV, AOC 8 ms for analog ... R2A, R2B 8 ms for discrete ... 800 Ohm , resolution 8 bits AOV configurable ... 470 Ohm , resolution 8 bits ... ) , < 5 V (state ... ... 10 mA at 5 V DC ... resistive load, 5 A at 250 ... resistive load, 5 A at 30 ... Time constant 5 ms for reference ...
Video: Using Network Management Card 2 (NMC2) bootmonitor to recover/upgrade firmware
Firmware revisions 5 . X . X , 6. X . X . ... device from v 5 . X . X to v6. X . X , please review ... Resolution ... Steps 4 - 5 ) and how ... Data bits 8 ... current BootMonitor version installed on the NMC ... ... Any Language Pack Installed !!! ... current BootMonitor version installed on the NMC ... ... the latest bootmon installed proceed with uploading ... ... Date : Apr 8 2014 ... Date : Apr 8 2014 ... : 10/ 28 /2013 10/ 28 /2013 00 ... 10/ 28 /2013 00 ...
How to enable .NET 2.0 on Windows 8.x and 10
Windows 8 . x and 10 ... .Net 2.0 is not pre- installed as part of the OS ... You will need to install the .Net 3.5 ... 5 . You should see .NET Framework 3.5 (includes .NET ... Framework 3.5 and click ok. Windows will proceed to install the service (downloading it from windows update if necessary). ... 2.0 you can now install PowerChute Personal Edition 3.0.2
How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
Resolution : ... 5 . Enter the correct number of attached battery packs. In order to setup the external battery packs, please key in as (Ah of battery) x (total number of batteries). ... Example 2: If there are 16 pcs of 100 AH batteries in series(for 5 KVA), the total AH number is 100 AH x 16 pcs=1600 AH
Video: Data Center Expert | Desktop Client Requirements, Download, & Installation
... to download and install the client application ... Resolution : ... discusses downloading and installing the Desktop Client ... ... 7, Windows 8 , or Windows ... Screen resolution should be set to at least 1024 x 768. ... 5 ) Run the downloaded execuatble file and follow the on-screen instructions. 6) Once the installation completes, you can launch to the Desktop Client using the Desktop Icon (if done during installation ) or the Start Menu Option for StruxureWare Data Center Expert #.#.#.


Résultats 1 - 10 de 95

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.