Consulter la FAQ



ACSC1XX Spare Parts List
CABLE ASSY TEMPERATURE SENSORS ( Rack Inlet) ... DRIVER BIT COMBO TORX t20/t30 (tool kit) ... EVAPORATOR FAN MODULE ASSY - 17 KW IR ... FITTING 1/8" BARB 10 -32 ... FITTING 1/8" BARB TEE (for air differential pressure switch) ... InRow RC/SC Filter 1/2" Washable - Spare Part (default) ... REAR DOOR ASSY - 17 KW ... TUBE 6 FT 10 " DIA FLEX DUCT ... 1U 19" Black Modular Toolless Airflow Management Blanking Panel - Qty 10
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... Support team) raru ACFXXX Rack Air Removal Unit AOS ... ACRD1XX, ACRD2XX InRow RD AOS v3.9.0 and higher Yes
Treck TCP/IP Vulnerabilities (ripple20)
Devices with an embedded ... Metered/Switched Rack PDUs, Rack Automatic Transfer Switches ... ... 100/160 kW UPS (PX2 ... ... 20/40 kW UPS APC Rack Power Distribution Units ... ... Metered/Switched Rack PDUs with embedded ... Rack Automatic Transfer Switches ... Rack Automatic Transfer Switches ... InRow Cooling for series ... InRow Cooling for series ... InRow Cooling for series acrd6xx and acrc6xx SKUs (ACRD2G) InRow Cooling Display for series acrd3xx (ACRC2G) InRow Cooling Display for series acrc3xx (RD3XX) InRow Cooling for series acsc1xx SKUs (SC2G) InRow Cooling for series acrd1xx and acrd2xx (ACRPTK2G) Ecoflair IAEC25/50 Air Economizer Display (EB2G)
acrd100 Operations and Maintenance Manual (Air-cooled)
acrd100, acrd101, Operations and Maintenance Manual, ACRD , Inrow , Aircooled
What are some of the applications for the InRow ACRD?
... applications for the InRow ACRD ? InRow Cooling The InRow RD is an InRow air conditioner designed for ... ... rejection options like air and fluid based ... The InRow RD is a ... The InRow RD allows for ... ... The closer the air conditioner is to ... the less likely air mixing of hot and cold air streams will occur ... The InRow RD is controlled ... modes using a rack inlet temperature probe ... ~ The InRow RD provides the ability to have two different media of heat rejection both using Direct expansion in addition to its capability of handling low loads of 2-20kw which ...
What are the different media that can be used with the InRow ACRD units?
The InRow ACRD can be used with refrigerant r410a alone in an air -cooled system.
What are the minimum load requirements for the ACRP DX?
InRow Cooling ... The InRow RP continually adjusts its cooling output to accommodate varying loads. The cooling output is determined by the difference between the supply air temperature setpoint and the actual supply air temperature as well as the airflow (for each of the cooling units in the cooling group if more than one cooling unit is present). ... Fully loaded, the nominal cooling capacity of the equipment is 29 kW . At its lowest speed, the equipment cooling capacity is approximately 10 kW but is is recommended to have at least 13 to 15 KW of load per unit.
APC Schneider Cooling Unit Identification
FM Air /Water/ ... Capacity KW Air Pattern ... Expansion A= Air Cooled E= Air Cooled Capacity KW Air Pattern Capacity KW Air Pattern Capacity KW Air Pattern Capacity KW Air Pattern ... Main A= Air Cooled Capacity KW Air Pattern ... ) A= Air Cooled Air Pattern 10 (2 Bay ... ... ) A= Air Cooled Capacity KW Air Pattern ... ) A= Air Cooled E= Air Cooled w/ ... R= Air Cooled w/ ... ... -5T Air Cooled or Air Pattern ... 0 A= Air Cooled SC= Air Cooled Self- ...
Where can I get support for APC and MGE Products?
Air Cooled Chillers Air Distribution Accessories ... Auto and Air Inverters ... Basic Rack PDU ... EcoBreeze Air Economizers ... InRow Chilled Water InRow Direct Expansion InRow Pumped Refrigerant ... Metered Rack PDU Metered-by-Outlet Rack PDU ... NetBotz Rack Access ... NetShelter Open Frame Rack Accessories ... Open Frame Racks ... Rack Air Distribution Rack Components Rack LCD Consoles Rack PDU Accessories Rack -mount Transfer Switches ... Room Air Distribution ... Switched Rack PDU ... Universal Mobile Device Batteries


Résultats 1 - 10 de 75

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.