Consulter la FAQ



Guidelines for installation of an acsc100, or acsc101
... to ducting and wiring. Ensure the room is insulated to minimize the influence of exterior heat loads.
DAC, Cancoil Installation Manual
... how to properly install a legacy DAC ... Install Resolution : Installation and Operating Instructions ... , medium and high temperature refrigeration applications. ... equipment, proper installation and set- ... ... cfm (of outside ventilation) per ... Installation Date __ ... Use high temperature silver solder or ... ... that will cause HEAT GAIN, it ... ... properly sized and installed to insure oil ... ... to minimize external heat gain and condensation ... ... risers should be installed with a trap ... ... have additional options installed . ... omponents have been installed . During periods of warm outdoor temperature, the liquid returns to the refrigerant receiver, and the condenser returns to full capacity.
Does my Smart-UPS have Equipment Protection Policy (EPP) coverage?
Any unit installed outside of the U.S. or Canada
What is the Difference between Glycol and Chilled water?
Resolution : ... The terms are used interchangeably in some cases, as many sites run chilled glycol through their chillers instead of straight water because the water lines are outside . The big difference is the heat transfer properties of glycol are not as good as straight water, so the equipment is de-rated depending on the glycol/water mixture.
What are the requirements for the acsc100 condenser unit
Resolution : ... to a total heat of rejection of ... ... possible to get higher temperatures . ... noted in the install manual the exhaust ... ... SC ducts directly outside ? The High Head Pressure Protection (HHPP) feature discussed earlier will proactively take steps to reduce the unit capacity, and thus the heat rejection requirement) in situations where the inlet temperature is too hot, or the airflow is overly restricted. ... Up to 0.25” (63 kPa) of additional static pressure beyond the standard duct kit installation can be tolerated with only a small impact on the condenser performance.
What is Peak Surge Current rating?
Resolution : ... The current is then boosted (say x+100a) remeasured, tested, remeasured, ... When the 100ma measurement falls outside the +/- 10% allowable window, the last kA measurement was valid. ... You will see a lower kA rating with the 2 impulse because the part has already been hammered once , it is warmed up , the material within the part has not completely 'reset' itself , and
What are your Cooling Product Energy efficiency rating (EER)?
Install Resolution : ... EER is generally calculated using a 95F outside temp and an inside (actually return air) temp of 80f and 50% relative humidity. ... = rated heating capacity output (kW)/ heating input power (kW)
What are the typical uses for an EcoAisle System
Install Resolution : ... the aisles with heat removed directly from ... The deployment of the Active Flow Controller more closely couples the cooling equipment to the IT heat load as it monitors the pressure inside vs outside the containment allowing the fan speed to be adjusted so that the right amount of air is being provided. ... The Active Flow controller looks at the pressure inside vs outside the aisle allowing it to quickly detect the dynamic load changes and send a control signal to adjust the airflow of the cooling equipment.
How to navigate through an Network Air FM unit display
Resolution : ... identify the hardware installed in this System ... ... the coil configuration installed in the Modules ... ... (PCIOMs) installed in the user ... Installation ... of air filters installed in the Modules ... ... recommended for typical installations . ... method used for heat rejection by the ... ... Rooms with small heat loads should use ... ... DX 60 Hz Installation ... and humidity probes installed must be supported ... ... To accommodate the heat of the rejection ... ... flow switch is installed : ... condenser valve is installed . ... isolation valve is installed in the coolant ... ... states to notify outside devices. ... If you have installed an Economizer automatic ...
Galaxy 5000, Galaxy 5500; Dust Covers
MGE Galaxy 5000, Galaxy 5500, Dust Cover, Input Wiring, Installation , foreign conductive particles,


Résultats 1 - 10 de 96

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.