Consulter la FAQ



Can the ar7708 Hot Air Recirculation Prevention Kit be used in a NetShelter SX Networking cabinet?
The front right hand rail uses foam blocks to seal the part of the rail not covered by an airflow duct.
When finger-style vertical cable managers are used in a 750mm wide NetShelter cabinet, is it possible to also block off the cable pass-thru openings in the mounting rails?
Using the finger-style vertical cable managers inside a NetShelter cabinet, designers need to know how to block hot air from recirculating through the rails. ... NetShelter SX ... If left open, hot air can recirculate through these holes. ... When there are finger style cable managers installed inside the 750mm wide NetShelter cabinet, AR7714 must be used to prevent hot air recirculation .
What should be checked if the NetShelter CX internal temperature exceeds expected levels? (5*C/41*F above room temp)
Cause: Fan issues, air recirculation , cabinet overloaded, intake/exhaust blocked , filter, wall clearance.
Do the Cisco Nexus 7700 series switches require a side airflow duct kit?
Customers ask if the Nexus 7700 series also requires side airflow duct kits . ... NetShelter SX ... The Cisco Nexus 7000 series switches utilize side airflow and required large volumes of air to cool properly. Duct kits are used to help the switches cool efficiently and prevent hot air recirculation .
How is the rackmount U-space of a NetShelter cabinet or rack identified?
NetShelter SX ... Incorrect placement of equipment can create airflow problems, like hot air recirculation .
Does APC offer a side airflow duct kit for the Cisco Nexus 7009, 7000 9-slot switch?
Cisco Nexus 7009 requires a side airflow duct kit when installed in a NetShelter cabinet. ... NetShelter SX ... This side airflow duct kit is designed specifically to allow the Cisco Nexus 7009 to install into the NetShelter cabinet and draw the additional air required to cool properly. ... The AR7725 draws air from the front and sides and guides it into the switches' air intakes. It also helps block hot air from recirculating to the front of the cabinet.
Can the horizontal cable troughs ar8008blk and ar8016ablk be used in conjunction with vertical cable managers ar7580a, AR7585 and AR7588?
NetShelter SX Wide cabinets, vertical cable management and horizontal troughs. ... All 750mm wide NetShelter SX cabinets: ar7580a, AR7585, AR7588, ar8008blk, ar8016ablk; all serial numbers. ... A customer wants to use both vertical finger-style vertical cable managers and horizontal cable troughs on the mounting rails of a 750mm wide NetShelter SX cabinet. ... Additionally, you may also use the roof brush strips AR7714 (5 per pack) to close off the holes in the cable managers and prevent hot air recirculation .
acf400 Spare parts break down
ACF115 APC Rack Air Removal Unit SX Fan Assembly 100-240v 50/60 Hz (All 4 fans and Electronics module included)
NetShelter CX Air Filters are Difficult to Install.
An incorrectly sized joining plate obstructs the air filters on the top of the cabinet. The bottom air filter is fine.
How to remove ceiling panels to access cabling on an EcoAisle
The duct system has an air - block system that can be removed with a thumbscrew.


Résultats 1 - 10 de 84

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.