Consulter la FAQ



Frequently Asked Questions for the new Lithium-ion Smart-UPS products.
Environment: All Lithium- ion models , All Serial Numbers
How do I retrieve logs from my Secure-UPS XP1K9NN42RCC Power management Unit?
All models , All Serial Numbers ... Set the default gateway of the NMC as the IP address of the computer. ... Default gateway : 192.168.1.2 (which is the IP address of the NMC) ... Link to some directions for establishing a hardwire connection between the network ports on a laptop and the PMU.
Where can I get support for APC and MGE Products?
Data Center Facility Power - PowerLogic ION Enterprise ... Desktop Notebook Stands ... Laptop Power Adapters ... Mobile Notebook Stands ... Notebook Security ... Power Ready Notebook Cases ... Replacement Notebook Batteries ... SurgeArrest Notebook ... Universal Notebook Batteries Universal Notebook Power Adapter
Video: How do I create a direct connection between a computer and a APC networked enabled product?
Laptop or computer with 10/100/1000 mbps Ethernet port ... Set the default gateway of the NMC as the IP address of the computer. ... Default gateway : 192.168.1.2 (which is the IP address of the NMC) ... After completing the above configuration, for our example, we are having the APC device look at the computer as its default gateway and having the computer look at the APC device as its default gateway .
Video: How do I configure APC Network Management Card network settings?
Some newer Smart-UPS models provide the capability to configure ... , subnet mask, and gateway using the front panel LCD display menu.
How do I recover the firmware on an ap5610, AP5615, AP5616 Digital IP KVM models?
... 3 and subnet mask of 255.0.0.0, no default gateway is required.
What if the StruxureO Gateway does not recognize my device?
... , and we are constantly working to grow our library of devices that we can model and monitor.
Which External Battery Pack (XLBP) and RBC is compatible with my Smart-UPS On-Line (SRT) model?
SRT48RMBP srt1000uxi-LI, srt1500uxi-LI Lithium Ion NMC chemistry No internal battery - uses external battery system NA See manual Blue XBP48RM1U ...
Samsung Lithium Ion Battery; alarm status-LED indication
Environment: All models , all serial numbers
Where can I find manual for Samsung Li-Ion Battery Solution
Environment: All models , All Serial numbers


Résultats 1 - 10 de 51

Vous n'avez pas trouvé ce que vous cherchiez ?

Contactez notre équipe client pour obtenir des informations sur l'assistance technique, l'assistance dédiée aux réclamations et plus encore.