{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

XU1K3LLXXRCC and XU2K0LLXXRCC Firmware Upgrade via NMC times out


Issue:

XU1K3LLXXRCC and XU2K0LLXXRCC Firmware Upgrade via Network Management Card times out and is unable to complete

Product Line:

Smart-UPS Industrial

Environment:

XU1K3LLXXRCC and XU2K0LLXXRCC, All Serial Numbers

Cause:

When upgrading the firmware via the Network Management Card there is a delay in transferring the data to the UPS.
This causes the update to time out and fail.
  • The time out error occurs while Receiving Firmware image is in progress.
  • The percentage at which the time out error occurs vary from unit to unit.


The LCD Display on the UPS will look like this:




The NMC Web interface will display this error:



Resolution:

If you experience this issue you can upgrade the UPS using a USB Thumb Drive rather than via the Network Management Card.
Instructions and the latest firmware image can be found in APC FAQ #FA402857

Note: Subsequent UPS firmware updates can be performed via the NMC, however, the time to perform the update may increase by 10 minutes.
En savoir plus
En savoir plus

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.