{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
How to re-launch PowerChute Network Shutdown CentOS 7, 8.1 Appliance initial setup menu
Issue:
Would like to re-launch the initial PowerChute Network Shutdown CentOS 7 Appliance setup.
Product Line:
PowerChute Network Shutdown v4.2, v4.3, v4.4
Environment:
PowerChute Network Shutdown v4.2, v4.3, v4.4 Appliance installed on VMware ESXi
NOTE: The PowerChute v4.4 Appliance is CentOS 8.1 based.
Cause:
Need to re-launch the initial setup menu
Solution:
Would like to re-launch the initial PowerChute Network Shutdown CentOS 7 Appliance setup.
Product Line:
PowerChute Network Shutdown v4.2, v4.3, v4.4
Environment:
PowerChute Network Shutdown v4.2, v4.3, v4.4 Appliance installed on VMware ESXi
NOTE: The PowerChute v4.4 Appliance is CentOS 8.1 based.
Cause:
Need to re-launch the initial setup menu
Solution:
- Log in to the PowerChute VM as root
- Enter the command systemctl enable initial-setup.service
- Enter the command touch /.unconfigured
- Enter the command init 6
En savoir plus
Gamme :
En savoir plus
Gamme :
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.