{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
PowerChute Network Shutdown cannot be installed on 32-bit systems
Issue:
PowerChute Network Shutdown v4.3 and higher (v4.3+) cannot be installed on 32-bit systems.
Product Line:
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
PowerChute v4.3 is bundled with JDK 11, which does not support 32-bit systems.
Solution:
If you require PowerChute on a 32-bit system, install PowerChute Network Shutdown v4.2, which is the last version to support 32-bit systems. To download PowerChute v4.2, visit the PowerChute Network Shutdown Product Page.
PowerChute Network Shutdown v4.3 and higher (v4.3+) cannot be installed on 32-bit systems.
Product Line:
PowerChute Network Shutdown
Environment:
All supported OS
Cause:
PowerChute v4.3 is bundled with JDK 11, which does not support 32-bit systems.
Solution:
If you require PowerChute on a 32-bit system, install PowerChute Network Shutdown v4.2, which is the last version to support 32-bit systems. To download PowerChute v4.2, visit the PowerChute Network Shutdown Product Page.
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.