{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
NetBotz 355 | Physical Description
Issue:
Physical Description of the NetBotz 355 and 355A
Product Line:
NetBotz version 3
- Wall Monitor 355
- Wall Monitor 355A
Environment:
NetBotz 355/355A (all firmware versions)
Resolution:
Physical Description - Front
Physical Description - Back
The complete NetBotz 455 Installation and Quick Configuration Manual can be found here.
Physical Description of the NetBotz 355 and 355A
Product Line:
NetBotz version 3
- Wall Monitor 355
- Wall Monitor 355A
Environment:
NetBotz 355/355A (all firmware versions)
Resolution:
Physical Description - Front
Item | Description | |
1 | Vented internal sensors | Vented opening for airflow, temperature, and humidity sensors. |
2 | Network link LED | Shows the status of the network connection. Blinks to indicate network traffic (green = connected at 10 Mbps; yellow = connected at 100 Mbps). |
3 | Power LED | Indicates whether the unit is receiving power (green = receiving power; dark = not receiving power) |
4 | Camera LED | Blinks steadily when the integrated camera is active. |
5 | Alert LED | Indicates the alert status of the system. When more than one alert exists, the most severe will be indicated. - Flashing once every eight seconds = Informational - Flashing one very four seconds = Warning - Flashing once every two seconds = Error - Flashing once every second = Critical - Flashing twice per second = Failure |
6 | Temperature display | - Displays the current temperature from 0 to 99 in Centigrade or Fahrenheit. The Temperature reading comes from the internal temperature sensor. If the temperature exceeds 99, the display will flash 99. - When the unit first receives power, displays the unique identifier number for one minute. - If an alert exists, flashes at the same rate as the Alert LED. - During firmware upgrade, displays 88. |
7 | Lens housing | Must be removed to change the focus of the integrated camera. |
Physical Description - Back
Item | Description | |
1 | Sensor ports (4) | Used for connecting APC by Schneider Electric sensors, third-party dry-contact sensors, and standard third-party 0-5 V sensors. Third-party dry-contact state sensors require the NetBotz Dry Contact Cable (NBES0304). Standard third-party 0-5 V sensors require the NetBotz 0-5 V Sensor Cable (NBES0305). |
2 | 10/100 Base-T network port | Provides for a 10/100 Base-T network connection and power through Power-over-Ethernet (PoE). (The appliance operates at 100 Base-T only.) Status and link LEDs indicate network traffic: - Status LED: blinks orange and green at start-up, then indicates the status of the network connection (solid green = IP address established; blinking green = attempting to obtain an IP address). - Link LED: blinks to indicate network traffic (green = connected at 10 Mbps; orange = connected at 100 Mbps). |
3 | USB port | Used to configure the appliance. |
4 | Reset | Used to restart the appliance. |
The complete NetBotz 455 Installation and Quick Configuration Manual can be found here.
En savoir plus
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.